Skip to main content
Associate II
Aug 5, 2025 2:26 AM UTC
Question

How does stm32H723 ADC ISR know which channel ?

I am just getting started with the stm32h723 ADC.    If I create a regular sequence group of several input channels, how does my ISR know which channel was sampled last (which channel's data is in the DR)?  I don't see this in the registers.

Thanks,

Mark 

This topic has been closed for replies.

7 replies

Tesla DeLorean
Guru
Aug 5, 2025 2:53 AM UTC

Typically you'd DMA a group of channels into an array, and then get an interrupt for some multiple of them.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
NiramasAuthor
Associate II
Aug 5, 2025 3:28 AM UTC

So I have to go down another rabbit hole to get my ADC data?   Is there a code example for the ADC-DMA transfer?

Tesla DeLorean
Guru
Aug 5, 2025 4:45 PM UTC

Not sure it's a rabbit hole, just not an 8-bit programming / 1-dimensional approach.

The concept is to allow for decimation of interrupt loading, and allow for more rapid/consistent cycling of the ADC, ie uniform sample rate so time-domain based analysis is workable.

Now if you want to sample individual channels on ADC1, ADC2, ADCn, then you can do that.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Technical Moderator
Aug 5, 2025 8:17 AM UTC

Hello @Niramas ,

You can get inspired from the "ADC DMA Transfer" example runs on STM32H743xx devices:

STM32CubeH7/Projects/NUCLEO-H743ZI/Examples/ADC/ADC_DMA_Transfer at master · STMicroelectronics/STM32CubeH7 · GitHub

This example can be easily tailored to any other supported device and development board.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
NiramasAuthor
Associate II
Aug 5, 2025 1:36 PM UTC

So are the examples for any STM32H7 variant applicable to the STM32H723?    I was only looking in the 723 examples folder.

ST Technical Moderator
Aug 5, 2025 3:50 PM UTC

You can use the ADC example from STM32H735 device which is a pin-to-pin compatible with STM32H723:

STM32CubeH7/Projects/STM32H735G-DK/Examples/ADC/ADC_DMA_Transfer at master · STMicroelectronics/STM32CubeH7 · GitHub

But always consult the datasheets and reference manuals for detailed comparison.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks