Skip to main content
Associate III
Mar 30, 2026 3:29 PM UTC
Solved

How does DCMI work with MCU & camera on different voltage levels?

Hiya. I'm having some trouble understanding how an STM32 MCU communicates with an image sensor via DCMI if they operate on different voltages.

My STM32U5Gxxx operates on 3V3, whereas my selected image sensor has its VDDIO at 2V8 (max input of 3V1). How can I make sure that all the signals I send to the sensor are at 2V8 instead of 3V3? Is there a certain VDDIOx pin to be tied?

Are there any reference designs or schematics that are helpful?

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Mar 31, 2026 9:19 AM UTC

Hello @f3l1xa88077 ;

 

I recommend you to use external level shifters for voltage level translation between the STM32 MCU and peripheral connected to the DCMI (such as image sensors at 2.8V).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

3 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Mar 31, 2026 9:19 AM UTC

Hello @f3l1xa88077 ;

 

I recommend you to use external level shifters for voltage level translation between the STM32 MCU and peripheral connected to the DCMI (such as image sensors at 2.8V).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Mar 31, 2026 9:21 AM UTC

@f3l1xa88077 wrote:

My STM32U5Gxxx operates on 3V3, whereas my selected image sensor has its VDDIO at 2V8


Why not just run your STM32 at 2V8, then ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KDJEM.1
ST Technical Moderator
Apr 13, 2026 3:59 PM UTC

Hello @f3l1xa88077 ;

 

Is your question answered?

If yes, please click on Accept as Solution on the reply which answered your question.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.