Skip to main content
Associate II
January 21, 2024
Question

How do we communicate Riverdi RVT70HSSNWCA0 Display with an external micro-controller/Nucleo board?

  • January 21, 2024
  • 2 replies
  • 1960 views

Hello everyone, Good day. Recently, I have bought a STM32 Display from Riverdi (model : RVT70HSSNWCA0) .
I would like to know how do I communicate an external STM32 Nucleo board with this display? For example : I want to read ADC Value from a potentiometer from the STM32 Nucleo Board and then have it be displayed on the Riverdi LCD. We are also using TouchGFX with Text Areas that have wildcards. How do we achieve something like this? Please provide kind support thank you best regards. 

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
January 21, 2024

Presumably you'd use the expansion connector and a UART to provide an inter-board communications channel. And a protocol or command/response type interaction over that channel.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
David Littell
Senior II
January 21, 2024

...and don't forget those magical things called "wires" to connect them!  ;)