Skip to main content
Explorer
Feb 6, 2025 3:10 PM UTC
Solved

How do STM32H753XIH6 and STM32L4S7AII6 verify memory contents?

Hello, does anyone know how these two components (STM32H753XIH6 and STM32L4S7AII6) verify that the data in both internal and external memories(Ram, Rom, Nor and Nand) are not corrupted?

Thanks for your help?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 6, 2025 3:16 PM UTC

Hello @Alex12 and welcome to the community,

In H7, the mechanism to check the memory consistency is the ECC either in internal RAM (RAM ECC) or the internal flash memory. For external memory only NAND mode is supporting ECC.

Refer to the AN5342 "How to use error correction code (ECC) management for internal memories
protection on STM32 MCUs "

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 6, 2025 3:16 PM UTC

Hello @Alex12 and welcome to the community,

In H7, the mechanism to check the memory consistency is the ECC either in internal RAM (RAM ECC) or the internal flash memory. For external memory only NAND mode is supporting ECC.

Refer to the AN5342 "How to use error correction code (ECC) management for internal memories
protection on STM32 MCUs "

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.