Skip to main content
Michael98006
Associate III
Jul 13, 2019 12:22 AM UTC
Solved

How do I set complimentary timer outputs in PWM mode to the same final state?

Is there a way to run N PWM cycles on TIM_CH1 and TIM1_CH1N (complimentary outputs of CH1) in OPM and set the final state of both outputs to low at the end of the final PWM cycle?

I'm using TIM1 in slave configuration with slave mode set to combined reset trigger mode with PWM mode 1 selected. My issue is that I end up with one of the two outputs set "high" when I want them both to be "low" at the end of the last PWM cycle.

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Jul 13, 2019 8:53 AM UTC

I don't think you can do it purely in hardware, but after the cycle ends, you can change the CHxN polarity by changing the respective CCxNP bit in TIMx_CCER. These bits are preloaded, if TIMx_CR2.CCPC is set, so you can write TIMx_CCER in advance before the last update event, and it will come into effect at the update event.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
Jul 13, 2019 8:53 AM UTC

I don't think you can do it purely in hardware, but after the cycle ends, you can change the CHxN polarity by changing the respective CCxNP bit in TIMx_CCER. These bits are preloaded, if TIMx_CR2.CCPC is set, so you can write TIMx_CCER in advance before the last update event, and it will come into effect at the update event.

JW

Michael98006
Associate III
Jul 16, 2019 5:05 PM UTC

I liked the idea of turning outputs on/off "by hand", but I went a step further and toggled the MOE bit on in the update event interrupt before the first PWM pulse and clearing the MOE bit on the update interrupt from the end of the last PWM cycle.