Skip to main content
LAdam.1
Associate II
February 19, 2021
Question

How do I select the right LSE for my STM32L433 when the LSE I have isn't working well?

  • February 19, 2021
  • 6 replies
  • 1703 views

I used an LSE component proven out on another design containing a STM32F412 for a new design using a STM32L433. The LSE part is Abracon ABS06-32.768kHz-6 which is listed in AN2867 as compatible with the L4 family. I'm using the HAL_RCCEx_EnableLSCO() function to pipe out my LSE signal and it is underwhelming. The duty cycle is roughly 40/60 and while the period is close, it's not as consistence as I would expect. I have tried changing the drive strength with the __HAL_RCC_LSEDRIVE_CONFIG() function. While the raw signal at the crystal looks better, the piped output doesn't improve when adjusting the drive strength. Drive strength is the only difference I can think of between the STM32F412 design and mine as the low drive for it is 1uA and the high drive for the STM32L433 is 630nA. Is there something else I am missing in software or in my crystal selection to explain the difference in performance?

The layout is tight and I also have CSS turned off per the errata notes.

Thanks,

Lauren

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
February 19, 2021

What load capacitors are you using?

ST's NUCLEO uses an NDK NK3215SA 32.768 Khz 6pF, with a pair of 6.8pF

That's probably on the high side, depending on what the stray capacitance looks like.

I'd probably try a couple of different values in your board/circuit as built and see if you can improve things that way.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Bowman32
ST Employee
March 1, 2021

Hi @LAdam.1​ 

I confirm the ABS06-32.768kHz-6 is compatible with STM32L4.

In deed, you can refer to AN2867, section "3.4 Oscillator transconductance" to calculate gmcrit. Then, check if Gm_crit_max > gmcrit. The Gm_crit_max is provided in STM32L4 datasheet, Table 57 "LSE oscillator characteristics (fLSE = 32.768 kHz)".

Also, you can refer to section "3.3 Load capacitance" to calculate the external capacitors.

What drive mode did you use?

Bouraoui

LAdam.1
LAdam.1Author
Associate II
March 2, 2021

I have tied every mode level, and they all gave about the same response. technically driving at anything about LOW will meet the gmcrit criteria. When I measure the piped out value of my LSE signal my average frequency is close to expected, but the range of frequencies is very wide at around 32.3kHz-33.3kHz.

Bowman32
ST Employee
March 3, 2021

To make sure that Gm_crit_max > gmcrit, I suggest to use Medium low drive mode.

What is the value of the used  external capacitors (CL1 and CL2)?

Bouraoui

LAdam.1
LAdam.1Author
Associate II
March 3, 2021

My CLs are 6.8pF. I tried lowering them without a noticeable difference in my output signal.

waclawek.jan
Super User
March 3, 2021

Tell us more about your hardware. What is the power supply? Are there any power components around? Or any high-frequency circuitry? Can you post the layout of the crystals surroundings?

JW