Skip to main content
Clement_Devevey
Associate II
March 8, 2022
Solved

How do I reach a component inside a container inside a scrollWheel from the view ?

Hi, I'm trying to change color of a component (circle) inside a container inside a scrollWheel.

This should occur when user press a button. The button is a component outside of scrollWheel. How can I reach this circle (inside a container inside a scrollWheel) from the view (where the button pressed function is) ?

Thanks

    This topic has been closed for replies.
    MM..1
    MM..1Best answer
    Super User
    March 8, 2022

    In container create method for change color.

    Then in button set an marker and in update callback use this marker and call item.changeclor...

    In button invoke callback update with call scrollwheel.itemChanged ...

    1 reply

    MM..1
    MM..1Best answer
    Super User
    March 8, 2022

    In container create method for change color.

    Then in button set an marker and in update callback use this marker and call item.changeclor...

    In button invoke callback update with call scrollwheel.itemChanged ...