Skip to main content
Associate
January 25, 2024
Question

how do I get the '.ld' link file for Flash

  • January 25, 2024
  • 5 replies
  • 3377 views

I have a question, how do I get the '.ld' link file for Flash, compared to the cmsis_device_f1 library cmsis_device_f4/Source/Templates/gcc/ directory that doesn't contain a `linker/` folder.

This topic has been closed for replies.

5 replies

TDK
January 25, 2024

If you make a CubeMX project, it will be in the top-level project directory. Something like STM32F411RETx_FLASH.ld.

You can also find it in any example projects. For example:

https://github.com/STMicroelectronics/STM32CubeF4/blob/master/Projects/STM32446E-Nucleo/Examples/I2C/I2C_TwoBoards_ComPolling/STM32CubeIDE/STM32F446RETX_FLASH.ld

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
zhbi98Author
Associate
January 25, 2024

Thanks for your explanation. I used CMake to build the project, so I needed to specifically look for this file

TDK
January 25, 2024

I mean, there are probably other ways, but it takes less than 5 minutes to make a cubemx project for the chip you have and generate code. Is it worth searching for other methods?

I searched the CubeMX repository and it came back with all the ld files in example projects. There may be another folder in there with them all but my brief search didn't turn it up.

"If you feel a post has answered your question, please click ""Accept as Solution""."
zhbi98Author
Associate
January 25, 2024

Thank you. I see