Skip to main content
JKo
Associate III
January 27, 2022
Question

How do I configure a NUCLEO-L4A6ZG LPUART1 to work with the ST-LINK Virtual COM port?

I've been trying to get the Virtual COM port from the ST-LINK on a NUCLEO-L4A6ZG working for 2 days now without luck. I've had no problem configuring the UART3 on a NUCLEO-F429ZI to work with the Virtual COM port. Only thing different is that the former is on the LPUART and the later is on the usual USART/UART. I've accounted for the different Baud Rate Register factor. How does the UART on the F103 of the ST-LINK detect the speed of the UART from the main board? Is it the UART on the ST-LINK restricted to a particular set of parameters? I've tried 115200,N81 and numerous other baud rates from 2400 and up without luck.

On the same NUCLEO-L4A6ZG I am able to configure the UART2 for successful communication to another board but the solution for the LPUART1 on this board eludes me.

I don't think I'm doing anything special with the LPUART1 on this board. In fact the NUCLEO-WL55JC1 I have also uses LPUART1 connected to the virtual com port and I have that working without issues.

How does the ST-LINK's F103 UART detect what baud, word length, stop bits, and parity is being used by the main board?

This topic has been closed for replies.

2 replies

Mike_ST
ST Technical Moderator
January 27, 2022

Hello,

LPUART1 is on GPIOG Pins 7 and 8, and without seeing your code, I would say you don't activate GPIOG pins that are relying on VDDOI2 power.

Please call  HAL_PWREx_EnableVddIO2(); function.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
JKo
JKoAuthor
Associate III
January 27, 2022

Thanks! That was it! I totally overlooked the PWR control component. I assumed my predecessor took care of such things on this when bringing up this MCU and I didn't find any bread crumb reminders in UM2179 nor RM0351 when reading the GPIO and LPUART portions that this needed to be done.