Skip to main content
Pedram
Associate III
Apr 5, 2019 2:41 PM UTC
Question

how config timer 1 to trigger timer 3 every fall edge on PWM channel 1 and channel 2

Hello everyone

how config timer 1 to trigger timer 3 every fall edge on PWM channel 1 and channel 2

This topic has been closed for replies.

1 reply

ST Technical Moderator
Apr 12, 2019 2:41 PM UTC

Hello @Pedram​ ,

It's not possible to trigger the timer 3 from timer 1 through channel 1 and channel 2 in the same time.

The source of trigger output of timer1 should be one of these:

  • Reset
  • Enable
  • Update
  • Compare Pulse (CC1IF)
  • Compare - OC1REF
  • Compare - OC2REF
  • Compare - OC3REF
  • Compare - OC4REF

You can refer to the "Timer synchronization" section in the reference manual relevant to your device.

Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks