Skip to main content
sasha
Associate III
Mar 19, 2019 11:49 AM UTC
Question

How can you enable TouchGFX within STMCube, using only internal memory (no FMC SDRAM)?

I want to create a project using an STM32F7 core, but don't want external memory - the MCU has more than enough memory for one or even two framebuffers in internal RAM. However - STMCube will not allow me to enable the Graphics Framework without FMC enabled. Is there away around this?

    This topic has been closed for replies.

    1 reply

    Shahrear
    Associate II
    Nov 5, 2022 1:06 AM UTC

    yes. its possible