Skip to main content
Diwakar Ragupathy Raj
Associate II
April 11, 2018
Question

How can i load .dfu file form the flas drive to my STM3241G-EVAL Evaluation board

Posted on April 11, 2018 at 15:24

Hello,

The demonstration application for the  STM3241G-EVAL Evaluation board was erased and I am trying to reprogram it back using USB flash drive. I followed the steps and still was not able to see progress in the LCD.

1). Jumper configuration was checked as per the datasheet. But for the boot mode the BOOT0 and BOOT1 should be 1<->2 but I see on the board there is either 0 or 1. what should I do now? and please help me what should be the BOOT0 and BOOT1 be set to ?

2). I copied the dfu file to the flash drive and then connected it to the board using the Micro-AB to standard receptacle A connector to the USB OTG HS pin. Is it correct ?

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    April 11, 2018
    Posted on April 11, 2018 at 15:48

    >>Is it correct ?

    No, that's not how DFU mode works. You need to run the DfuSe utility from Windows.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Diwakar Ragupathy Raj
    Associate II
    April 11, 2018
    Posted on April 11, 2018 at 16:31

    i downloaded the Dfuse Utility to my computer but then the board is not recognised 

    Tesla DeLorean
    Guru
    April 11, 2018
    Posted on April 11, 2018 at 17:14

    The BOOT0 switch should be in the 1 position (right), the System Loader will want to use the USB-FS connector.

    I'm sure most of this stuff is documented.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..