Skip to main content
Associate
Apr 12, 2024 5:27 PM UTC
Question

How can i link 2 wifi+mcu boards with one as the access point?

Hi community!

I am working on a hobby project (custom pcb) where i need my stm32 mcu to communicate with a wifi chip, which will send data to a second pcb which is a usb dongle with a similar mcu+wifi setup, only that wifi chip acts as an access point only the first mentioned wifi chip can access and send/receive data from.

How would i go about this and what wifi chip is recommended for it?

I am planning to use the STM32H745IIT6. (maybe a bit overkill, but i need it to process a lot of stuff).

Another thing is that i want to connect 16 small boards, (which contain a BMM350 and a BMI323) to the MCU via I2C, because the STM32H745IIT6 has 4 I2C Interfaces. Is this feasable to do?

 

I appreciate the assistance.

Thanks,

This topic has been closed for replies.

7 replies

Pavel A.
Apr 12, 2024 7:52 PM UTC

There are wi-fi modules that support both AP and station modes, for example this one is used in some ST eval. boards: MXCHIP EMW3080B. And there are ESP8266 and other ESP chips. 

 

 

 

JTechAuthor
Associate
Apr 13, 2024 7:07 AM UTC

Thanks!

I will probably use the ESP8266EX.

Any tips on the second part of the question?

For some more clarification, the STM32H745IIT6 has 4 I2C interfaces i'm using, and it also has 4 SPI interfaces i could use. Would i be better of using The I2C interfaces, the SPI interfaces, or a combination of both?

AScha.3
Super User
Apr 13, 2024 8:23 AM UTC

Hi,

1 - ESP8266  is ok (but ESP32-S2-mini  : i would think about using it and no H7 , cpu here 32bit/240MHz (almost same power as an H7 ), and 2MB RAM , 4MB flash + SPI, I2C etc... at 2,50 !

https://de.aliexpress.com/item/1005005977413920.html

2 - How long will be connection line to this gyro/magnetic sensors ? screened ?

If you feel a post has answered your question, please click on " Best Answer ".
JTechAuthor
Associate
Apr 13, 2024 12:13 PM UTC

Hi,

1) Thanks for the suggestion! Will definately look into that.

2) Quite long since the 16 sensor packages are individual motion trackers that are relatively far appart

JTechAuthor
Associate
Apr 13, 2024 4:09 PM UTC

Ah i understand now, thanks for the clarification.

So SPI would be able to handle up to 16 devices (split across 4 SPI interfaces) right?