Skip to main content
taz1000
Associate II
July 25, 2016
Question

How can I have 4MHz I2C signal ?

  • July 25, 2016
  • 1 reply
  • 645 views
Posted on July 25, 2016 at 03:50

I know that I2C's official speed is 100KHz (Standard Mode), 400KHz (Fast Mode), 1MHz (Fast Mode Plus).

But, in my lab application, I need to implement 4MHz I2C signal. 

I had used FPGA logics to achieve 4MHz I2C signal. But, to make simple

system I'm changing it to STM32F207. But, I can't make 4MHz I2C. 

I'm using 0.8K Ohm Pull-Up resistor on SCL and SDA to achieve 4MHz. 

I generated the reference code with CubeMX. With this code, 

1MHz I2C can be made very easily. Changing the initial speed setting is it. 

That was all. 

But, if I tried to change the speed to 2MHz or 4MHz, the signal is not

generated properly. 

Can you make examples to generate 4MHz I2C ?

    MX_I2C3_Init ( );

    HAL_I2C_Master_Transmit ( );

I tried to change options, and to modife code in Transmit();

I had put more condition checkings and delays, but it didn't make change. 

I can clear the HW issue if there is. 

So, please let me have your reference codefor 4MHz I2C. 

Thanks, 

Best Regards, 

Danny 
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    July 25, 2016
    Posted on July 25, 2016 at 17:25

    Consider using a more appropriate interface, like SPI?

    Check the divisor/prescaler options in the reference manual, you probably can't get to 4 MHz, but it seems like a bad plan anyway, rethink.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..