Skip to main content
Ccui.1
Associate II
Jan 12, 2020 2:49 AM UTC
Solved

How can I get voucher code for P-L496G-CELL 02 after accidentally erased the startup FW?

I accidentally overwrote the FW loaded by ST for P-L496G-CELL 02. So I cannot access the voucher code. Is there any way to retrieve the voucher code?

This topic has been closed for replies.
S.Ma
S.MaBest answer
Principal
Jan 12, 2020 11:01 AM UTC

I used to play with this kit in the past, and here was the original "restore my kit" binary.

It might not be the latest one. It's here in case it helps.

Connect STLink, use it as USB Memory stick and drag and drop/flash the bin file if the board is up and ready, configured as in the insert card inside pages pictures.

2 replies

S.Ma
S.MaBest answer
Principal
Jan 12, 2020 11:01 AM UTC

I used to play with this kit in the past, and here was the original "restore my kit" binary.

It might not be the latest one. It's here in case it helps.

Connect STLink, use it as USB Memory stick and drag and drop/flash the bin file if the board is up and ready, configured as in the insert card inside pages pictures.

Ccui.1
Ccui.1Author
Associate II
Jan 12, 2020 2:01 PM UTC

It works. Thanks.