How can i get the clock signal from SPI_SCK?
Hello. I want ask something that drive to me mad.
Using STM32F769NIH for control external ADC(AD7192) with SPI interface
SPI6 for SPI communication(PG13 -> SCK, PA6 -> MISO, PG14 -> MOSI)
nChip Select controlled by PI13
clock enable to all use(PORT A, G, I) and SPI6 also
setting to SPI6 and initialize it
but I can't get the clock signal from PG13(SPI6_SCK)
how can i get the clock signal? what is wrong?
p.s i check PIN and AF from ref. if i mistake it, plz tell me
//////////////////////////////////////////////////////code/////////////////////////////////////////////////////////
GPIO_InitTypeDef GPIO_InitStruct;
SPI_HandleTypeDef hspi; __HAL_RCC_GPIOI_CLK_ENABLE(); //nCS PIN GPIO_InitStruct.Pin = GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOI, &GPIO_InitStruct); __HAL_RCC_SPI6_CLK_ENABLE(); //spi gpio __HAL_RCC_GPIOG_CLK_ENABLE(); // PG13 ------> SPI6_SCK GPIO_InitStruct.Pin = GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF5_SPI6; HAL_GPIO_Init(GPIOG, &GPIO_InitStruct); __HAL_RCC_GPIOA_CLK_ENABLE(); // PA6 ------> SPI6_MISO GPIO_InitStruct.Pin = GPIO_PIN_6; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF8_SPI6; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); __HAL_RCC_GPIOG_CLK_ENABLE(); // PG14 ------> SPI6_MOSI GPIO_InitStruct.Pin = GPIO_PIN_14; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF5_SPI6; HAL_GPIO_Init(GPIOG, &GPIO_InitStruct); hspi.Instance = SPI6; hspi.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256; hspi.Init.Direction = SPI_DIRECTION_2LINES; hspi.Init.CLKPhase = SPI_PHASE_1EDGE; hspi.Init.CLKPolarity = SPI_POLARITY_LOW; hspi.Init.DataSize = SPI_DATASIZE_8BIT; hspi.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi.Init.TIMode = SPI_TIMODE_DISABLE; hspi.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi.Init.CRCPolynomial = 7; hspi.Init.NSS = SPI_NSS_SOFT;// hspi.Init.NSSPMODE = SPI_NSS_PULSE_DISABLE; hspi.Init.Mode = SPI_MODE_MASTER; if(HAL_OK != HAL_SPI_Init(&hspi)) { printf('INIT_ERROR'); }while(1)
{
}
/////////////////////////////////////////////end/////////////////////////////////