Skip to main content
JBrad.4
Associate II
November 15, 2020
Question

How can I extract SensorTile accelerometer data from default firmware over bluetooth?

  • November 15, 2020
  • 0 replies
  • 496 views

I've just purchased a STEVAL-STLKT01V1 and successfully connected it to the BLE App which extracts the various data well. I need to develop an application that connect to the SensorTile in the same way over bluetooth. Ideally I would not need to flash any custom firmware, but just use what is already loaded on there. The application would be built in Max https://cycling74.com.

The problems I am running into now are:

1) The sensortile is visible on a number of windows, android machines but not on a 2015 Macbook pro that supports BLE 4.2 or a 2013 Macbook Air. When I try to pair the devices the SensorTile is never visible.

2) If/When I get the sensortile connected to my laptop - how can I extract a specific set of data?

This topic has been closed for replies.