Skip to main content
antonius
Associate III
December 26, 2013
Question

How can I define PORTE on STM32 as D0-D7 on LCD?

  • December 26, 2013
  • 3 replies
  • 787 views
Posted on December 26, 2013 at 14:38

Guys,

How can I define PORTE on STM32 as D0-D7 on LCD?

I have more than 8bits on PORTE,

on AVR for example PORTA = data, how can I do it on STM32 ?

any ideas ?

thanks
    This topic has been closed for replies.

    3 replies

    lowpowermcu
    Associate III
    December 26, 2013
    Posted on December 26, 2013 at 16:23

    Hi rick,

    You can refer to ST library.

    The ports are defined as GPIOA, GPIOB, GPIOC....

    and evey port has 15 pins: Pin 0, Pin 1,.... Pin 15

    Tesla DeLorean
    Guru
    December 26, 2013
    Posted on December 26, 2013 at 16:44

    GPIOE->BSRR = data | ((~data & 0xFF) << 16); //??

    or

    GPIOE->ODR = (GPIOE->ODR & 0xFF00) | data;
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    antonius
    antoniusAuthor
    Associate III
    December 26, 2013
    Posted on December 26, 2013 at 16:57

    I wrote, please have a look and correct me :

    //LCD Define

    #define lcd_data_pin  GPIOE

    #define rs    GPIO_Pin_8

    #define rw    GPIO_Pin_9

    #define en    GPIO_Pin_10

    void GPIO_Configuration(void)

    {

      GPIO_InitTypeDef GPIO_InitStructure;

     

      //RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOB , ENABLE);

           RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOE | RCC_APB2Periph_GPIOA, ENABLE);                         

        GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7

        | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10;

        GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

        GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

        GPIO_Init(GPIOE, &GPIO_InitStructure);

    }

    void lcd_cmd(unsigned char cmd){

        //lcd_data_pin = cmd ;

        GPIO_Write(lcd_data_pin, cmd);

         GPIO_WriteBit(lcd_data_pin, en, Bit_SET);

         GPIO_WriteBit(lcd_data_pin, rs, Bit_RESET);

         GPIO_WriteBit(lcd_data_pin, rw, Bit_RESET);

        //en=1;

        //rs=0;

        //rw=0;

        vTaskDelay(10);

        GPIO_WriteBit(lcd_data_pin, en, Bit_RESET);

        //en=0;

        

    }