Skip to main content
naceur2311
Associate II
May 21, 2013
Question

How can i configure Timer1 to generate an interrupt with 50 Hz ???

  • May 21, 2013
  • 7 replies
  • 1894 views
Posted on May 21, 2013 at 20:37

I want to measure the frequency of an input signal with the STM32F4 Discovery Board. But i want to configure Timer 1 (in mode Input capture) to generate an interrupt every 50 Hz (or any other fixed value). How can i do this ???

Thank you.

    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    May 21, 2013
    Posted on May 21, 2013 at 20:55

    So set up the timebase period and prescaler to divide the source clock down to 50 Hz. Factor in a manner of your choosing. Enable the Update interrupt

    For an 84 MHz TIMCLK

    Prescale = 28 - 1;

    Period = 60000 - 1;

    Your input compare will be a modulo 60000 value now. Ticks will be in 3 MHz units, ie 333.333 ns, update at 20 ms (50 Hz)

    50 * 28 * 60000 = 84000000
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Jessy J
    Associate III
    June 11, 2018
    Posted on June 11, 2018 at 11:58

    HELLO

    Turvey.Clive

    ‌

    I want to ask you how to know the value of TIMCLK please ??

    I activated timer 14 for mode compare output no output mode and I want to set its interrupt every 100 ms

    thank you for your reply in advance

    Tesla DeLorean
    Guru
    June 11, 2018
    Posted on June 11, 2018 at 13:41

    Review the Clock Tree in the Reference Manual, the TIMCLK is derived from the APB Clock the TIM being used is attached too.

    ie if APB1, in all cases other than the DIV1 setting the TIMCLK = APB1CLK * 2;

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    henry.dick
    Associate II
    June 11, 2018
    Posted on June 11, 2018 at 12:07

    '

    But i want to configure Timer 1 (in mode Input capture) to generate an interrupt every 50 Hz (or any other fixed value). '

    since you are using the input capture mode to generate interrupts, you just need to configure the timer to interrupt on every rising / falling edge and feed it a 50Hz signal.

    'How can i do this ???'

    by coding to the datasheet.

    the other approach highlighted earlier is incorrect.

    Jessy J
    Associate III
    June 11, 2018
    Posted on June 11, 2018 at 12:14

    henry.****

    ‌

    I want to ask you how to know the value of TIMCLK please ??

    henry.dick
    Associate II
    June 11, 2018
    Posted on June 11, 2018 at 22:57

    For what you are trying to do, the value in timclk is irrelevant - basically the in out pulse train determines the maximum frequency of (input capture) interrupts.

    If you insist, two easy ways to know the value of timclk:

    1. Go through the datasheet and your code.

    2. Run your code in a debugger and inspect the register.

    Jessy J
    Associate III
    June 14, 2018
    Posted on June 14, 2018 at 10:27

    Turvey.Clive

    ‌

    For an 84 MHz TIMCLK Prescale = 28 - 1;

    Period = 60000 - 1;

    Your input compare will be a modulo 60000 value now. Ticks will be in 3 MHz units, ie 333 ns, update at 20 ms (50 Hz)

    50 * 28 * 60000 = 84000000

    In cubMX in the configuration shall we write 28 as prescale value or 27 ?? same as periode value please ??

    thank you for your reply