Question
How Can I Code For Boot-loader In STM32F030K6T6 Using I2C Protocol With Anther Board of STM32F030K6T6???
Hello ,
I Am Working With Two STM32F030K6T6 Board ,Which is Used As a Boot-loader application With I2C protocol.
So I Can Communicate Small Data But Some How I Can Not Communicate A Long Data To Transmitted or Received From Master To Slave Or Slave To Master .
I Have Try Both the The Method Using Blocking mode And Non-Blocking Mode .
So Please suggest How To Make a Code For Long Data Transmission Using I2C Protocol In Both Board .