Skip to main content
SBenn.2
Associate
December 30, 2023
Solved

High-speed data transfer to memory mapped peripheral using FMC via DMA?

Is it possible to burst transfer a block of data from STM32 internal Flash/SRAM to an external memory mapped peripheral device with an SRAM style interface i.e. Address, Data, CS and R/W using the FMC fed via DMA?

This topic has been closed for replies.
TDK
TDKBest answer
December 30, 2023

Yes, you can transfer between internal memory and external memory using DMA. Configure FMC so that the external memory is mapped to an address and then set up a memory-to-memory transfer to or from that address.

"If you feel a post has answered your question, please click ""Accept as Solution""."

1 reply

TDK
TDKBest answer
December 30, 2023

Yes, you can transfer between internal memory and external memory using DMA. Configure FMC so that the external memory is mapped to an address and then set up a memory-to-memory transfer to or from that address.

"If you feel a post has answered your question, please click ""Accept as Solution""."