Question
High level at the outputs of PA9 and PA10 after reset. STM32G030K8
After resetting, the output of PA9 and PA10 of the STM32G030K8 microcontroller is high. These pins are not initialized, according to the datasheet after reset they should have the function of an analog input. Once configured, they function normally as outputs.
It is important for me that after the reset and before the adjustment, the outputs are like analog inputs.