high current consumption with stm32g474
I have about 250 mikroAmpere current consumption in shutdown mode.
used board: NUCLEO-G474RE, nothing except ammeter connected to the board.
code to shutdown:
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_DisableWakeUpPin (PWR_WAKEUP_PIN2_HIGH);
/* Clear all related wakeup flags */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_PWR_EnableWakeUpPin (PWR_WAKEUP_PIN2_HIGH);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_PWREx_EnterSHUTDOWNMode();
the same code on a nucleo f411 schows 2 uA as expected. only the G474 board show this high current.
our application board with g474 show the same high current.
if I heat the board up, the current is not increasing!
what can be the problem?
Is something special with g474?
thanks
Martin