Skip to main content
josef2
Associate III
Jun 17, 2021 9:28 AM UTC
Solved

Hi, where I find the Binary STM32H745I_OSCILLO_SG_CM4.bin for the STM32H745-Discovery Demonstration best regards Josef

..

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jun 17, 2021 10:34 AM UTC

Hi @josef2​ ,

The Full demonstration binary files are available from the STM32H745I-DISCO page, in the Compiled demos section (Please refer to the direct link).

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Mike_ST
ST Technical Moderator
Jun 17, 2021 10:21 AM UTC

Hello,

should be the binary you get after you compiled the following project available inside the H7 firmware package:

STM32Cube_FW_H7_V1.9.0\Projects\STM32H745I-DISCO\Demonstrations

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Imen.DBest answer
ST Technical Moderator
Jun 17, 2021 10:34 AM UTC

Hi @josef2​ ,

The Full demonstration binary files are available from the STM32H745I-DISCO page, in the Compiled demos section (Please refer to the direct link).

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks