Skip to main content
chaitanya jasti
Associate II
Feb 25, 2017 5:55 AM UTC
Solved

Hi what is boot0 in stm32

Posted on February 25, 2017 at 06:55

hi we are using STM32L152RET6.what is boot0 meant for and what should i connect

    This topic has been closed for replies.
    RomainR.
    RomainR.Best answer
    ST Employee
    Mar 3, 2018 8:28 PM UTC
    Posted on March 03, 2018 at 20:28

    Yes BOOT0 tied to 0V

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    11 replies

    S.Ma
    Principal
    Feb 25, 2017 8:06 AM UTC
    Posted on February 25, 2017 at 09:06

    First time the STM32 is powered up (and reset line is released), an internal bootcode (bootloader) will kick in first and check if the flash is blank. If the flash is blank, the bootloader will enable and listen for some peripherals (some UART/I2C/SPI/USB) to communicate with the external world as a mean to download and flashing the device.

    If the flash is not blank, the user code in the flash will start.

    If boot0 is tied high, the bootloader will assume the flash is blank.

    Another way to program the flash of the microcontroller is by debugger (ST Link) through SWD or JTAG.

    On STM8 MCU due to low pincount, the bootloader does not have a boot0 pin and instead the bootloader will be listening for communication for a single second after reset line is released.

    waclawek.jan
    Super User
    Feb 25, 2017 11:09 AM UTC
    Posted on February 25, 2017 at 11:09

    First time the STM32 is powered up (and reset line is released), an internal bootcode (bootloader) will kick in first and check if the flash is blank. If the flash is blank, the bootloader will enable

    This does not apply universally to all STM32, only to the newer ones - in particular, in the 'L1 this is not implemented.

    For an exhaustively detailed list, see Table 2. Bootloader activation patterns in AN2606.

    JW