Skip to main content
adham.1
Associate
Mar 28, 2022 5:24 AM UTC
Solved

Hi,Is it possible to load hex file of STM32F746ZGT6 in to STM32F756ZGT6? need to program directly using utility

A hex file generated from STM32F746ZGT6 is it compatible with STM32F756ZGT6?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 28, 2022 8:18 AM UTC

Hello,

The two devices have the same memory mapping and same features except STM32F756 features a Crypto hardware acceleration. So yes, you can load a hex file generated for STM32F746ZGT6 to STM32F756ZGT6 device.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 28, 2022 8:18 AM UTC

Hello,

The two devices have the same memory mapping and same features except STM32F756 features a Crypto hardware acceleration. So yes, you can load a hex file generated for STM32F746ZGT6 to STM32F756ZGT6 device.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
adham.1
adham.1Author
Associate
Mar 28, 2022 9:17 AM UTC

thank you so much...!

mƎALLEm
ST Technical Moderator
Mar 28, 2022 9:35 AM UTC

You're welcome. Please close this thread by clicking "Select as best" in the answer.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.