Question
Hi , I would like to know if there is a way to use DMA to get the TIM1 advanced timer update events ? I can successfully trigger an IRQ but having problems setting a DMA to trigger on every update. I am using STM32 L4 MCU.
I am using the advanced timer TIM1 on STM32L476RG MCU. I have configured the timer in slave reset mode as given in section 30.3.26 of the reference manual. The counter resets every rising edge. I want to use this mode to measure low frequencies such as 500 Hz. The way I am trying to do that is by using the timer update event and calculating the total counter value using that
I would like to know how to configure and use DMA for timer update event(counter rollover in up counting mode) ?