hi i am using STM32f746zg microcontroller with CANBUS i want to establish communication between CAN1 and CAN2 where CAN1(master) will send and CAN2(slave) should receive. CAN1 is transmitting perfectly but it is not receiving at CAN2 ..
can anyone help me with the code ....thanks in advance
here is my code
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 0 */
/* USER CODE END CAN1_Init 0 */
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 30;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_15TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
/* USER CODE END CAN1_Init 2 */
}
/**
* @brief CAN2 Initialization Function
* @param None
* @retval None
*/
static void MX_CAN2_Init(void)
{
/* USER CODE BEGIN CAN2_Init 0 */
/* USER CODE END CAN2_Init 0 */
/* USER CODE BEGIN CAN2_Init 1 */
/* USER CODE END CAN2_Init 1 */
hcan2.Instance = CAN2;
hcan2.Init.Prescaler = 30;
hcan2.Init.Mode = CAN_MODE_NORMAL;
hcan2.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan2.Init.TimeSeg1 = CAN_BS1_15TQ;
hcan2.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan2.Init.TimeTriggeredMode = DISABLE;
hcan2.Init.AutoBusOff = DISABLE;
hcan2.Init.AutoWakeUp = DISABLE;
hcan2.Init.AutoRetransmission = DISABLE;
hcan2.Init.ReceiveFifoLocked = DISABLE;
hcan2.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN2_Init 2 */
/* USER CODE END CAN2_Init 2 */
}
void can1_filter(void)
{
CAN_FilterTypeDef filter1;
filter1.FilterActivation=CAN_FILTER_ENABLE;
filter1.FilterBank=0;
filter1.FilterFIFOAssignment=CAN_RX_FIFO0;
filter1.FilterIdHigh=0x0000;
filter1.FilterIdLow=0x0000;
filter1.FilterMaskIdHigh=0x0000;
filter1.FilterMaskIdLow=0x0000;
filter1.FilterMode= CAN_FILTERMODE_IDMASK;
filter1.FilterScale=CAN_FILTERSCALE_32BIT;
filter1.SlaveStartFilterBank=13;
if(HAL_CAN_ConfigFilter(&hcan1,&filter1)!=HAL_OK)
{
Error_Handler();
}
}
void can2_filter(void)
{
CAN_FilterTypeDef filter2;
filter2.FilterActivation=CAN_FILTER_ENABLE;
filter2.FilterBank=0;
filter2.FilterFIFOAssignment= CAN_RX_FIFO0;
filter2.FilterIdHigh=0x0000;
filter2.FilterIdLow=0x0000;
filter2.FilterMaskIdHigh=0x0000;
filter2.FilterMaskIdLow=0x0000;
filter2.FilterMode= CAN_FILTERMODE_IDMASK;
filter2.FilterScale=CAN_FILTERSCALE_32BIT;
filter2.SlaveStartFilterBank=14;
if(HAL_CAN_ConfigFilter(&hcan2,&filter2)!=HAL_OK)
{
Error_Handler();
}
}
void can(void)
{
CAN_TxHeaderTypeDef TxHeader;
uint32_t TxMailbox;
uint8_t usr_msg[8];
usr_msg[0]=0xAF;
//usr_msg[1]=0xAD;
TxHeader.DLC=2;
TxHeader.RTR= CAN_RTR_DATA ;
TxHeader.IDE= CAN_ID_STD;
TxHeader.StdId= 0x65;
if(HAL_CAN_AddTxMessage(&hcan1,&TxHeader,usr_msg,&TxMailbox)!=HAL_OK)
{
Error_Handler();
}
while(HAL_CAN_IsTxMessagePending(&hcan1,TxMailbox));
HAL_GPIO_WritePin(GPIOB, LD1_Pin, GPIO_PIN_SET);
}
void RX(void)
{
CAN_RxHeaderTypeDef RxHeader;
uint8_t rcv_msg[10];
while(HAL_CAN_GetRxFifoFillLevel(&hcan2,CAN_RX_FIFO0)<1);
if(HAL_CAN_GetRxMessage(&hcan2,CAN_RX_FIFO0,&RxHeader,rcv_msg)!=HAL_OK)
{
//HAL_CAN_GetError(&hcan2);
Error_Handler();
}
HAL_GPIO_WritePin(GPIOB, LD2_Pin, GPIO_PIN_SET);
}