Hi everyone, I want to help for selecting STM32 Micro-controller for my application(Ultra Low Power)
1. Hardware requirement
I/O - Minimum 12
SPI, I2C, UART, WDT, ADC
2. MEMORY NEEDS
MINI 32K FLASH & 4K RAM
3. Ultra low power & Power Mode
power down current < 1 uA
I/O Pin to retain it's state
Package :- LQFP
Free software libraries and examples available with the STM32Cube MCU Package.
I can easily interface with any sensors and I can do any other development easily.
Available on STM32CubeMX and Also compatible with Arduino.
So Please Help me to selecting a perfect STM32 MC, According to my requirement, which STM32 Micro-controller is good for me?