Skip to main content
waclawek.jan
Super User
Sep 19, 2019 8:31 AM UTC
Question

Here we go again with suffixed parts (STM32G474RET6U)

From the 'G4 DISCO UM2577:

This board features a specific STM32 device version, which allows the operation of any bundled commercial

stack/library available. This STM32 device shows a "U" marking option at the end of the standard part number

and is not available for sales.

In order to use the same commercial stack in his application, a developer may need to purchase a part number

specific to this stack/library. The price of those part numbers includes the stack/library royalties.

I can find no mention of the U suffix on the 'G474 product folder webpage, nor in the DS.

ST, can you please properly document it this time?

Thanks,

JW

This topic has been closed for replies.

14 replies

waclawek.jan
Super User
Aug 20, 2021 8:29 AM UTC

D suffix in 'L0 meaning "BOR disabled".

(specifically in 'L05x and 'L07x) 

S suffix in 'L031 in QFN28 means "different pinout from the non-S suffix", but it also means "the same pinout as 'L011 and 'F031 in QFN28". Nice.

0693W00000LvZgtQAF.png 

JW