Skip to main content
MCosm.3
Associate
Nov 19, 2021 6:11 AM UTC
Solved

Help with Led blinking - STM32F7508-DK

Hi folks, first off all I'd say to that I'm really new to MCU and for some silly reason I went for a STM32F7508-DK as my first board of STM3. With that being said, I'm asking for help on why my Led blinking code is not working,

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2021 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under Ultimate Liberty license
 * SLA0044, the "License"; You may not use this file except in compliance with
 * the License. You may obtain a copy of the License at:
 * www.st.com/SLA0044
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 /* USER CODE BEGIN 2 */
 
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 
	 // My code
	 HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_1);
	 HAL_Delay(500);
 
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 216;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 9;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Activate the Over-Drive mode
 */
 if (HAL_PWREx_EnableOverDrive() != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOI_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOI, GPIO_PIN_1, GPIO_PIN_RESET);
 
 /*Configure GPIO pin : PI1 */
 GPIO_InitStruct.Pin = GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);
 
 /*Configure GPIO pin : PI11 */
 GPIO_InitStruct.Pin = GPIO_PIN_11;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

I disabled all the pins that I'm not using and just enabling PI1 for the LED and PI11 for the button. The program is supposed to blink the LED every 500ms but the LED just remains on.

When I try to debug the program seems to get stuck in this function: (within stm32f7xx_hal.c)

HAL_StatusTypeDef HAL_Init(void)
{
 /* Configure Instruction cache through ART accelerator */ 
#if (ART_ACCLERATOR_ENABLE != 0)
 __HAL_FLASH_ART_ENABLE();
#endif /* ART_ACCLERATOR_ENABLE */
 
 /* Configure Flash prefetch */
#if (PREFETCH_ENABLE != 0U)
 __HAL_FLASH_PREFETCH_BUFFER_ENABLE();
#endif /* PREFETCH_ENABLE */
 
 /* Set Interrupt Group Priority */
 HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
 
 /* Use systick as time base source and configure 1ms tick (default clock after Reset is HSI) */
 HAL_InitTick(TICK_INT_PRIORITY);
 
 /* Init the low level hardware */
 HAL_MspInit();
 
 /* Return function status */
 return HAL_OK;
}

Any help is really welcomed.

Thanks.

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 19, 2021 9:28 AM UTC

Welcome. @MC.4osmes​, to the community!

as far as I can see, your only code that you put in main.c is:

HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_1);
HAL_Delay(500);

It is a simple one and works perfectly on the STM32F7508-DK.

Do you know, which function in HAL_Init() is causing this issue?

You don't need to set a breakpoint, because HAL_Init() is called in the beginning inb main(). Just:

  • start debugging using F11,
  • wait until the debugger runs and points to HAL_Init() in main.c
  • step over using F6 until you find the function that is stuck

Could you please share the .ioc file so we can check your clock settings too?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 19, 2021 9:28 AM UTC

Welcome. @MC.4osmes​, to the community!

as far as I can see, your only code that you put in main.c is:

HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_1);
HAL_Delay(500);

It is a simple one and works perfectly on the STM32F7508-DK.

Do you know, which function in HAL_Init() is causing this issue?

You don't need to set a breakpoint, because HAL_Init() is called in the beginning inb main(). Just:

  • start debugging using F11,
  • wait until the debugger runs and points to HAL_Init() in main.c
  • step over using F6 until you find the function that is stuck

Could you please share the .ioc file so we can check your clock settings too?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MCosm.3
MCosm.3Author
Associate
Nov 19, 2021 9:34 PM UTC

Thanks for your suggestion Peter, I found out that was getting stuck in the HAL_Delay() call then found out that I needed to add two lines to the following function within stm32f7xx_it.c

void SysTick_Handler(void)
{
 
 /* USER CODE BEGIN SysTick_IRQn 0 */
	HAL_IncTick();
	HAL_SYSTICK_IRQHandler();
 
 /* USER CODE END SysTick_IRQn 0 */
 /* USER CODE BEGIN SysTick_IRQn 1 */
 
 /* USER CODE END SysTick_IRQn 1 */
}

Thanks again.

Amel NASRI
ST Technical Moderator
Nov 26, 2021 4:20 PM UTC

Hi @MC.4osmes​ ,

Welcome to the STM32 Community :)

If you still need some getting started resources related to STM32 product, I suggest you to refer to the step by step tutorials.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Associate II
Jun 27, 2023 10:17 PM UTC

I runned into same issue in my case everything stucks at MX_GPIO_Init -> HAL_TIM_IRQHandler and doesn't move any futher (code of @mc_it.4osmes​ doesn't help for me)