Skip to main content
vekariyamitul
Associate
June 13, 2012
Question

Help to understand default program that comes with stm32 discovery

  • June 13, 2012
  • 4 replies
  • 1656 views
Posted on June 13, 2012 at 17:13

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    June 13, 2012
    Posted on June 13, 2012 at 17:43

    Try looking at the SysTick_Handler() in STM32F4-Discovery_FW_V1.1.0\Project\Demonstration\stm32f4xx_it.c

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    vekariyamitul
    Associate
    June 13, 2012
    Posted on June 13, 2012 at 18:58

    thanks man......really appreciate your help......

     but is it necessary to use TIM4? I've tried to use STM_EVAL_LEDOn(LEDn) function instead of using timer compatator, but it didn't work. Can you tell me how can we just turn on led without blinking or using TIM4?

    Tesla DeLorean
    Guru
    June 13, 2012
    Posted on June 13, 2012 at 20:55

    I'd start by not calling TIM4_Config(), which changes the GPIO pins to AF (Alternate Funtion) mode. The LEDs LD3, LD4, LD5, and LD6 are conveniently behind TIM4 channels, but you can leave them in GPIO mode.

    You should then be able to use :

    STM_EVAL_LEDOff(LED4);

    STM_EVAL_LEDOn(LED4);

    STM_EVAL_LEDToggle(LED4);

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    osama
    Associate III
    January 9, 2013
    Posted on January 09, 2013 at 19:33

    The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6mQ&d=%2Fa%2F0X0000000bvH%2FyNwfcJyTBuAazH3fmIGaj7oDo0aXzyvGMn6rqUu0K1I&asPdf=false