Skip to main content
tranvanduy
Associate
April 6, 2014
Question

[HELP] STM32F4 generate PWM 3 channel shift phase 120 degree!

  • April 6, 2014
  • 40 replies
  • 6117 views
Posted on April 06, 2014 at 06:30

Hi all!

I want to control 3 phase motor (I get HDD motor from old HDD), and now I can generate 3 PWM signal on 3 channels but they are same, not

shift phase

120 degree!

Please help me!

I use STM32F4 discovery board and Keil!

Thanks all
    This topic has been closed for replies.

    40 replies

    Tesla DeLorean
    Guru
    April 6, 2014
    Posted on April 06, 2014 at 06:48

    If you need 3 Phase at 50/50 duty, you could use toggle mode, programming the phase shift into the ''Pulse'' field

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    April 6, 2014
    Posted on April 06, 2014 at 07:21

    // STM32F4-Discovery TIM4 Tri-Phase Output PD.12, PD.13 and PD.14 - sourcer32@gmail.com
    #include ''stm32f4xx.h''
    //******************************************************************************
    void RCC_Configuration(void)
    {
    /* enable peripheral clock for TIM4 */
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
    /* GPIOD clock enable */
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
    }
    //******************************************************************************
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /* GPIOD Configuration: TIM4 on PD12/PD13/PD14 LED */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOD, &GPIO_InitStructure);
    /* Connect TIM4 pin */
    GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_TIM4); // PD12 TIM4_CH1
    GPIO_PinAFConfig(GPIOD, GPIO_PinSource13, GPIO_AF_TIM4); // PD13 TIM4_CH2
    GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_TIM4); // PD14 TIM4_CH3
    }
    //******************************************************************************
    void TIM4_Configuration(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_OCInitTypeDef TIM_OCInitStructure;
    int Prescaler, Period;
    Prescaler = ((SystemCoreClock / 2) / 20000); // 20 KHz timebase, assumes APB1 H/4 TIMCLK4 H/2
    Period = 20000 / 1; // 1 Hz - 1 second on, 1 second off duty
    // The toggle halves the frequency, a phase shift of 90 degrees (1/4) is 180 degrees (1/2)
    /* Time base configuration */
    TIM_TimeBaseStructure.TIM_Period = Period - 1;
    TIM_TimeBaseStructure.TIM_Prescaler = Prescaler - 1;
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
    /* Output Compare Toggle Mode configuration: Channel 1, 2 & 3 */
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    TIM_OCInitStructure.TIM_Pulse = (Period / 6); // CH1 60 + 0 Degrees
    TIM_OC1Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = (Period / 6) + (Period / 3); // CH2 60 + 120 Degrees
    TIM_OC2Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = (Period / 6) + ((Period * 2) / 3); // CH3 60 + 240 Degrees
    TIM_OC3Init(TIM4, &TIM_OCInitStructure);
    /* TIM4 enable counter */
    TIM_Cmd(TIM4, ENABLE);
    }
    //******************************************************************************
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    TIM4_Configuration();
    while(1); /* Infinite loop */
    }
    /**************************************************************************/
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    while (1)
    {}
    }
    #endif
    /**************************************************************************/

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    tranvanduy
    Associate
    April 16, 2014
    Posted on April 16, 2014 at 10:30

    Hi Clive, I tested and your code is ok, and now I want to invert direction of motor, I know I have to update period to Ch1 = period*2/3 and Ch3 = period/3, but I don't know how to update period value.

    Now i change TIM4_Configuration() function to 2 function: TIM4_Configuration_left() TIM4_Configuration_right() Would you have another way for me update the period to invert direction?! Thanks you very much!

    *****************************************
     TIM_OCInitStructure.TIM_Pulse = (Period / 6); // CH1 60 + 0 Degrees
     TIM_OC1Init(TIM4, &TIM_OCInitStructure);
     
     TIM_OCInitStructure.TIM_Pulse = (Period / 6) + (Period / 3); // CH2 60 + 120 Degrees
     TIM_OC2Init(TIM4, &TIM_OCInitStructure);
     
     TIM_OCInitStructure.TIM_Pulse = (Period / 6) + ((Period * 2) / 3); // CH3 60 + 240 Degrees
     TIM_OC3Init(TIM4, &TIM_OCInitStructure);
     *****************************************

    Tesla DeLorean
    Guru
    April 16, 2014
    Posted on April 16, 2014 at 16:12

    The period relates to the speed. To reverse the phase relationship, you'd presumably swap ch 1 & 3 settings.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    tranvanduy
    Associate
    April 16, 2014
    Posted on April 16, 2014 at 18:30

    oh, I'm sorry. I want to talk about the pulse.

    The pulse is set in TIM4_Configuration() function, and I want update the pulse for 3 channel: Left:

    *****************************************
    TIM_OCInitStructure.TIM_Pulse = 0; // CH1 0 + 0 Degrees
    TIM_OC1Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = 0 + (Period / 3); // CH2 0 + 120 Degrees
    TIM_OC2Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = 0 + ((Period * 2) / 3); // CH3 0 + 240 Degrees
    TIM_OC3Init(TIM4, &TIM_OCInitStructure);
    *****************************************

    Right:

    *****************************************
    TIM_OCInitStructure.TIM_Pulse = 0+ ((Period * 2) / 3); // CH1 0 + 240 Degrees
    TIM_OC1Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = 0 + (Period / 3); // CH2 0 + 120 Degrees
    TIM_OC2Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = 0; // CH3 0 + 0 Degrees
    TIM_OC3Init(TIM4, &TIM_OCInitStructure);
    *****************************************

    But I don't know how to update it in while loop, so now I write 2 function TIM4_Configuration_left()

    void TIM4_Configuration_left(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_OCInitTypeDef TIM_OCInitStructure; //dung cho PWM
    int Prescaler, Period;
    Prescaler = ((SystemCoreClock / 2) / 20000); // 20 KHz timebase, assumes APB1 H/4 TIMCLK4 H/2
    Period = 20000 / 1; // 1 Hz
    /*
    Prescaler = ((SystemCoreClock / 2) / 360000); // ~360 KHz timebase, assumes APB1 H/4 TIMCLK4 H/2
    Period = 36000; // ~10 Hz -> ~ 5 Hz
    */
    /* Time base configuration */
    TIM_TimeBaseStructure.TIM_Period = Period - 1; 
    TIM_TimeBaseStructure.TIM_Prescaler = (Prescaler - 1)/20; //10 Hz
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
    /* Output Compare Toggle Mode configuration: Channel 1, 2 & 3 */
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; 
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    TIM_OCInitStructure.TIM_Pulse = 0; // CH1 0 + 0 Degrees
    TIM_OC1Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = 0 + (Period / 3); // CH2 0 + 120 Degrees
    TIM_OC2Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = 0 + ((Period * 2) / 3); // CH3 0 + 240 Degrees
    TIM_OC3Init(TIM4, &TIM_OCInitStructure);
    TIM_ARRPreloadConfig(TIM4, ENABLE); 
    /* TIM4 enable counter */
    TIM_Cmd(TIM4, ENABLE);
    }

    and TIM4_Configuration_right()

    void TIM4_Configuration_right(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_OCInitTypeDef TIM_OCInitStructure; //dung cho PWM
    int Prescaler, Period;
    Prescaler = ((SystemCoreClock / 2) / 20000); // 20 KHz timebase, assumes APB1 H/4 TIMCLK4 H/2
    Period = 20000 / 1; // 1 Hz
    /*
    Prescaler = ((SystemCoreClock / 2) / 360000); // ~360 KHz timebase, assumes APB1 H/4 TIMCLK4 H/2
    Period = 36000; // ~10 Hz -> ~ 5 Hz
    */
    /* Time base configuration */
    TIM_TimeBaseStructure.TIM_Period = Period - 1; 
    TIM_TimeBaseStructure.TIM_Prescaler = (Prescaler - 1)/20; //10 Hz
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
    /* Output Compare Toggle Mode configuration: Channel 1, 2 & 3 */
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; 
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    TIM_OCInitStructure.TIM_Pulse = 0+ ((Period * 2) / 3); // CH1 0 + 240 Degrees
    TIM_OC1Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = 0 + (Period / 3); // CH2 0 + 120 Degrees
    TIM_OC2Init(TIM4, &TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_Pulse = 0; // CH3 0 + 0 Degrees
    TIM_OC3Init(TIM4, &TIM_OCInitStructure);
    TIM_ARRPreloadConfig(TIM4, ENABLE); 
    /* TIM4 enable counter */
    TIM_Cmd(TIM4, ENABLE);
    }

    And the main program:

    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    while(1) /* Infinite loop */
    {
    TIM4_Configuration_left();
    delay();
    TIM4_Configuration_right();
    delay();
    }
    }

    But I think it 's not good, I think to have another way to invert direction without reconfig the Timer. Hope you see what I want to say! hihi Thank you!
    Tesla DeLorean
    Guru
    April 16, 2014
    Posted on April 16, 2014 at 19:38

    The total reconfiguration seems rather unnecessary.

    Why wouldn't you simply reprogram the TIMx->CCR1, TIMx->CCR2, TIMx->CCR3 in the Update interrupt?

    I would recommend you read the chapter(s) on the TIM peripherals in the reference manual.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    aspire
    Visitor II
    April 24, 2014
    Posted on April 24, 2014 at 02:30

    Hi Mr Clive1,,how to update n generate PWM for delay 120 degree with ADC input..?like as Voltage divider or etc...

    Tesla DeLorean
    Guru
    April 24, 2014
    Posted on April 24, 2014 at 04:19

    Yes, I'm not completely sure what the question is, when language fails consider a diagram.

    It should be possible to trigger ADC conversions on various ADC units/channels using TIM channels/updates. The associativity between ADC and TIM triggers can be found in the Reference Manuals for the parts.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    aspire
    Visitor II
    May 6, 2014
    Posted on May 06, 2014 at 18:24

    hmm,thanks Mr Clive.

    by the way, what is other technique if we will generated 3 phasa PWM but it is not use toggle mode..? this PWM use for trigger dc - dc converter.

    aspire
    Visitor II
    May 6, 2014
    Posted on May 06, 2014 at 18:26