Skip to main content
mustapha_menhou
Associate II
March 25, 2013
Question

help STM32-P103 RS232

  • March 25, 2013
  • 4 replies
  • 766 views
Posted on March 25, 2013 at 22:18

Hi i

 would like

to use the circuit

MAX3232

(

RS232

adapter

) to connect two 

PORT

RS232

with this

 circuit 

using just

TX and RX

only

if possible

this experience?

?

?

?

?

and thank you 
    This topic has been closed for replies.

    4 replies

    Andrew Neil
    Super User
    March 25, 2013
    Posted on March 25, 2013 at 23:02

    There seems to be a language barrier here. Perhaps it would be easier to explain your requirement with a diagram...?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    mustapha_menhou
    Associate II
    March 25, 2013
    Posted on March 26, 2013 at 00:15

    Here is a

    PDF

    that

    represents

    my problem

    if

    possible to do this

    configuration?

    ??

    ________________

    Attachments :

    Doc1.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1An&d=%2Fa%2F0X0000000bjO%2FMxvFcOji_FYohzLHw5WB39F3L3WIkazQ.unp2P0.vmY&asPdf=false
    Andrew Neil
    Super User
    March 26, 2013
    Posted on March 26, 2013 at 07:47

    By ''STM32-P103'' I assume you mean this:

    https://www.olimex.com/Products/ARM/ST/STM32-P103/

    Note that it has one RS232 port already - so you only need to add one other.

    Study the documentation to see where the other UART port pins can be accessed on the various connectors on the board...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    March 26, 2013
    Posted on March 26, 2013 at 09:31

    I see you have also posted the same question in a different thread:

    /519d41ef

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.