Skip to main content
Channamallesh Hiremath
Associate II
May 11, 2018 5:48 AM UTC
Solved

Help needed to understand stm32F3 discovery board schematics

Posted on May 11, 2018 at 07:48

On the stm32F3 discovery boards, where do pins on CN3 get connected when CN4 jumpers are on and off. 

Schematics says, CN4 jumpers on, will select discovery. Off means ST-LINK is selected. 

If I take CN4 off, then CN3 pin2 is not connected to PA14 of st32f303 device. 

I have to have CN4 on for PA14 to get connected to pin2 of CN3.

Please help me. 

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    May 11, 2018 6:12 AM UTC
    Posted on May 11, 2018 at 08:12

    The pins in CN3 always connect to the output pins of the ST-LINK STM32F103, CN4 connects the ST-LINK to the F3 target on the board.

    If you want to program an external target STM32 via CN3 then you need to disconnect the on-board target by removing the CN4 jumpers. You do this so you don't have TWO targets with SWDIO/SWCLK pins that clash and cause it so neither can be programmed/debugger properly.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    1 reply

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    May 11, 2018 6:12 AM UTC
    Posted on May 11, 2018 at 08:12

    The pins in CN3 always connect to the output pins of the ST-LINK STM32F103, CN4 connects the ST-LINK to the F3 target on the board.

    If you want to program an external target STM32 via CN3 then you need to disconnect the on-board target by removing the CN4 jumpers. You do this so you don't have TWO targets with SWDIO/SWCLK pins that clash and cause it so neither can be programmed/debugger properly.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..