Skip to main content
bee
Associate
August 19, 2013
Question

Help me fix my code.ADC with STM32F303VC

  • August 19, 2013
  • 0 replies
  • 438 views
Posted on August 19, 2013 at 07:20

I want read ADC of STM32F303VC then display status  on three LED (If ADC>1000 LED red bright,ADC<500 LED green bright and extant LED ogrange bright) programmed code below,but i don't find error.Thanks everyone!

#include ''main.h''

__IO uint16_t  AD= 0,DA=0, ADC1ConvertedVoltage = 0, calibration_value = 0;

__IO uint32_t TimingDelay = 0;

ADC_InitTypeDef       ADC_InitStructure;

ADC_CommonInitTypeDef ADC_CommonInitStructure;

GPIO_InitTypeDef      GPIO_InitStructure;

/////////////////////////////////////////////////////////////////////////////////////////

int main(void)

{

 

  RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2);

  

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);

      

  /* Setup SysTick Timer for 1 µsec interrupts  */

  if (SysTick_Config(SystemCoreClock / 1000000))

  { 

    /* Capture error */ 

    while (1)

    {}

  }

////////////////LED///////////////////////////////////

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9| GPIO_Pin_10| GPIO_Pin_11;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOE, &GPIO_InitStructure);

///////////////////////ADC///////////////////////////////

  /* GPIOC Periph clock enable */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

  /* Configure ADC Channel2 as analog input (Pin 1 of Port A-PA1) */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  ADC_StructInit(&ADC_InitStructure);

////////////////////////////////////////////////////////////////////////////////////////////////

  /* Calibration procedure */  

  ADC_VoltageRegulatorCmd(ADC1, ENABLE);

  

  /* Insert delay equal to 10 µs */

  Delay(10);

  ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);

  ADC_StartCalibration(ADC1);

  

  while(ADC_GetCalibrationStatus(ADC1) != RESET );

  calibration_value = ADC_GetCalibrationValue(ADC1);

     

  ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;                                                                    

  ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode;                    

  ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;             

  ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot;                  

  ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0;          

  ADC_CommonInit(ADC1, &ADC_CommonInitStructure);

  

  ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable;

  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; 

  ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0;         

  ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None;

  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

  ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable;   

  ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable;  

  ADC_InitStructure.ADC_NbrOfRegChannel = 1;

  ADC_Init(ADC1, &ADC_InitStructure);

   ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 1, ADC_SampleTime_4Cycles5);

//////////////////////////////////////////////////////////////////////////////////////////////  

  

  ADC_Cmd(ADC1, ENABLE);

  /* wait for ADRDY */

  while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));

  

  

  ADC_StartConversion(ADC1);   

  

  /* Infinite loop */

  while (1)

  {

    /* Test EOC flag */

    while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);

    AD =ADC_GetConversionValue(ADC1);

 

    DA =(AD *3300)/0xFFF;

//////////////////////////////////////////////////////////////////////////////////// 

while(AD>1000)

 { 

GPIO_SetBits(GPIOE,GPIO_Pin_9);

      }

while(AD<500)

 {

GPIO_SetBits(GPIOE,GPIO_Pin_11);

      }

GPIO_SetBits(GPIOE,GPIO_Pin_10);

  }

}

////////////////////////////////////////////////////////////////////////////////////

void Delay(__IO uint32_t nTime)

  TimingDelay = nTime;

  while(TimingDelay != 0);

}

and my project here:

http://www.mediafire.com/download/zbuszqh91kkah6f/ADC.7z
    This topic has been closed for replies.