Skip to main content
mehmet.karakaya
Associate III
August 31, 2013
Question

help - F103 window watchdog

  • August 31, 2013
  • 3 replies
  • 678 views
Posted on August 31, 2013 at 21:45

hello dear forum,

I am trying to setup window watchdog on F103

I want wwdg to be reset in a window of 8 - 12 milisecond

I set wwdg prescaler to 2 so wwdg timer is counting every 0.227 microsecond

the enable line sets the counter to 117 -> so117-63 = 25 milisecond max timeout value

if I set

WWDG_SetWindowValue(117);

the wwdg works fine

however if I set a lover value for example 95

WWDG_SetWindowValue(95);

so 117-95 = 22 * 0.227 = 5 ms minimum timeout valuethe processor never gets out of reset

I tried with 78 --> 8.8 ms still resetting the uC

what am I doing wrong ?

why doesnot it work according to the manual ?

thank you

RCC_APB1PeriphClockCmd(RCC_APB1Periph_WWDG, ENABLE);

.....................

TIM_Init()

// timer sets to 10 ms period - its IRQ routine sets TIMERJOB variable

WWDG_SetPrescaler(WWDG_Prescaler_2);

WWDG_SetWindowValue(117);

// <---- the problem here

WWDG_Enable(117);

while

(1) {

if

(TIMERJOB) { TIMERJOB=0;

WWDG_Enable(117);

.................other jobs ;

}

#wwdg-f103

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    September 1, 2013
    Posted on September 01, 2013 at 02:08

    I'd recommend you try two things.

    1) Replace the WWDG kick in you main loop, and instead toggle a GPIO. Confirm on a scope that you don't ever exceed 12 ms, for whatever reason. ie stuck in an interrupt for too long. If you have a logic analyzer do this also when you have the WWDG running and capture the case when it resets.

    2) Try an Enable value that is always lower than the window value, ie N-1, or 116

    The 12 ms number looks good for a 36 MHz bus on APB1
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mehmet.karakaya
    Associate III
    September 1, 2013
    Posted on September 01, 2013 at 16:36

    hello thanks for the answer

    I am sure the timer ticks at 10 ms interval - I checked it before with oscilosscope

    TIM_TimeBaseStructure.TIM_Period = 7200; 
    TIM_TimeBaseStructure.TIM_Prescaler = 100; 
    TIM_TimeBaseStructure.TIM_ClockDivision = 0; 
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; 
    TIM_TimeBaseInit(TIM6, &TIM_TimeBaseStructure); 

    the only thing I suspect is that the timers first interrupt comes right after I

    volatile uint8_t TIMERJOB=0
     ............
     TIMInit() 

    i.e it doesnot wait 10 ms for the first overflow of timer is it posible ?
    Tesla DeLorean
    Guru
    September 1, 2013
    Posted on September 01, 2013 at 16:59

    I'm sure the hardware TIM ticks correctly too, but that's not the point.

    You're not kicking the WWDG in the TIM Update service routine.

    The interrupt service may be delayed or stalled. The foreground loop may not run in a timely fashion.

    I would start by looking at other aspects of your system before blaming the WWDG
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..