Hello! I'm using STM32L422 and I'm having trouble with setting up the PLL above certain frequencies. Are there any specific configuration requirements when setting up PLL at high frequencies?
I use 8MHz crystal as the input for the PLL. I'm using a timer and a LED to verify frequency, aka the LED should blink at 1Hz. Everything works fine until 48MHz, after which the STM seems to fail - led doesn't blink and the debugger does not know where is the program counter. The register values indicate that yes, the frequency should be 80MHz, just before it is enabled. And also if I increase the PLLR (output prescaler) to divide to 40MHz, then everything starts to work again.. I also have tried using the HSI16 as input and the same result.