Skip to main content
dkim.3
Associate II
March 17, 2023
Question

Hello, I'm using hal_delay in my code. The part where I used hal_delay to take a waveform using an oscilloscope is a little strange. Can Hal_delay cause waveform problems?

  • March 17, 2023
  • 2 replies
  • 788 views

..

    This topic has been closed for replies.

    2 replies

    Foued_KH
    ST Employee
    March 17, 2023

    Hello @dkim.3​ 

    I think you have the same issue as reported here : HAL_Delay() is not working properly!!! (st.com)

    Foued

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    dkim.3
    dkim.3Author
    Associate II
    March 17, 2023

    It seems to me that it is about time. But my problem is with waveforms. When you meet delay after always being high in the waveform, the high value drops for a while and then transmits the bit you want to transmit. Since there is only a delay function in the meantime, I am guessing that there is something disturbing the waveform in the delay function, and I wonder if this is right. If it is a factor that cannot be disturbed, I will further study it.