Skip to main content
Norhane BENKAHLA
Associate II
January 10, 2018
Question

Hello, i have Discovery kit LoRa, i will implement my algorithm in this cards for tests, and i want to know if i can make changes in the part of the header of the message lora? if it's possible to do this, where can i do it ? Thanks Norhane BENKAHLA

  • January 10, 2018
  • 2 replies
  • 822 views
Posted on January 10, 2018 at 14:44

Hello, i have Discovery kit LoRa, i will implement my algorithm in this cards for tests, and i want to know if i can make changes in the part of the header of the message lora? if it's possible to do this, where can i do it ? Thanks Norhane BENKAHLA

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    January 10, 2018
    Posted on January 10, 2018 at 18:51

    Can we please not put the entire question in the summary line?

    LoRa or LoRaWAN ?

    What are you sending? What portion do you want to change? What would be the purpose of changing it?

    You could change the preamble bytes but it would make it incompatible with other COTS devices.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Norhane BENKAHLA
    Associate II
    January 10, 2018
    Posted on January 10, 2018 at 20:02

    I want to change a header of lorawan. I want to add another fields for testing my algorithm. The fields will indicate different informations about a device, for exemple priority of device, the time on air that the device will consume during 1 cycle. Is ti possible to add new fields in the header of frame ? How can i do this ? 

    Thanks