When I am trying to flash to controller, I am getting an error 'Internal Command Error' and then it says 'Flashing is failed in Cortex M0'. So, what could be the problem?
The debugger can talk to the chip or loses connectivty. Check you have the right pins connected and device doesn't power down. On the PC side make sure you have picked the right debugger and flash algorithm.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Where, exactly, are you getting that error? What software are you using? What hardware are you using?
Has it ever worked, or is this a 'new' problem?
Anuraag P wrote:
it says
What says?
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ie, is this a fundamental issue, or is it just something to do with Keil...
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.