Skip to main content
kunal burman
Visitor II
March 19, 2021
Question

Hello, I am designing a wireless DMM , where i need to measure the capacitance from 1 nF to few Farads and Resistance 2 wire resistance measurement (till 40 MOhm) using stm32? Please can anyone guide me for the same

  • March 19, 2021
  • 1 reply
  • 912 views

..

    This topic has been closed for replies.

    1 reply

    Andrew Neil
    Super User
    March 19, 2021

    So what have you tried so far?

    Where are you stuck?

    Do you understand the basic principles of measuring capacitance & resistance?

    People have been measuring these fundamental physical properties for centuries; so the principles are well known and well documented - they aren't going to be changed because you're using an STM32

    When you say "wireless", what, exactly, do you mean?

    Clearly the measurements themselves will require wires to connect to the things being measured

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.