Skip to main content
JHIEB.1
Associate
April 26, 2023
Solved

Hello, How does reducing the bit count of the ADC peripheral affect the quoted SINAD in the datasheet, if at all?

For example, I wish to use ADC1 (14 bits max) of STM32U575 at 12 bits, single ended. The datasheet guarantees a minimum of 68 dB for the SINAD, does this figure get reduced from 14 bits to 12 bits? If so, by how much?

Thanks,

Joel

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
April 29, 2023

yes, basically your right.

  • to be 100% sure, try both and check result.
  • on average, the 14b data should have lower noise
If you feel a post has answered your question, please click on " Best Answer ".

5 replies

Billy OWEN
ST Employee
April 28, 2023

Hi @JHIEB.1​ 

The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

Regards,

Billy

JHIEB.1
JHIEB.1Author
Associate
April 28, 2023

Hi again,

I did some digging on the topic and the answer seems quite simple: If I set the resolution to 12 bits, the SNR for an ideal ADC should be 12x6.02+1.76 = 74 dB, which is clearly more than the 68 dB min SINAD figure, so I won't lose any accuracy by doing so. Actually, as long as the resolution is at least equal to the worst case ENOB, I won't lose any (AC) accuracy. Can anybody confirm?

Thanks,

Joel

AScha.3
AScha.3Best answer
Super User
April 29, 2023

yes, basically your right.

  • to be 100% sure, try both and check result.
  • on average, the 14b data should have lower noise
If you feel a post has answered your question, please click on " Best Answer ".
JHIEB.1
JHIEB.1Author
Associate
April 29, 2023

Thanks!