Hello Guys, I am facing problem in STM32H7 DMA. I had written code to receive the data from UART in DMA mode. In that i am transmitting the data in Polling mode and receiving in DMA mode.
In this at first time only data is receiving after that code is not executing RxCmplt call back function.
Hardware: For testing I had shorted the both TX and RX pins together of STM32H743I EVAL board.
UART Config : Baud rate = 9600,DataSize = 8bit,Mode = Tx and Rx, Stop Bits = 1, Parity = None, DMA_RX = Circular,DMA1_Stream0
Please help me if any one know the solution.