Skip to main content
AAl-A.1
Visitor II
January 15, 2021
Question

Hello everybody, i have a discovery board STM32F407VG. i worked with it quite well. but wenn i connect the board i get message The interface firmware FAILED to reset/halt the target MCU

  • January 15, 2021
  • 2 replies
  • 588 views

..

This topic has been closed for replies.

2 replies

Vangelis Fortounas
Associate II
January 15, 2021

Hello

In STLink settings , try to "connect under reset" and use "Hardware Reset" as reset option.

Update also the STLink firmware to the latest version

Tesla DeLorean
Guru
January 15, 2021

Figure you have reconfigured PA13 PA14 or gone to sleep.

Try erasing using other tools or strap BOOT0 to VDD so it doesn't run your code. ​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..