Hell Has Frozen Over, NFC CR95HF Library Evaluates True -> False
Ok, I've seen some strange things in my day but this has got to be the most insane thing I've come across. Need a brilliant person to try to help me explain this:
The NFC CR95HF library is a work in progress but we are using it anyways. The chip detects all types of tags EXCEPT the ones we want to use, Type 4. So debugging the code I come across this situation.
if ((tagsToFind&TRACK_NFCTYPE2) || (tagsToFind&TRACK_NFCTYPE4A))
{
PCD_FieldOff();
HAL_Delay(5);
ISO14443A_Init( );
if(ISO14443A_IsPresent() == RESULTOK)
{
if(ISO14443A_Anticollision() == RESULTOK)
{
if ( ( ( ISO14443A_Card.SAK & 0x60 ) == 0x00 ) && ( tagsToFind & TRACK_NFCTYPE2 ) ) /* TT2 */
return TRACK_NFCTYPE2;
else if ( ( ( ISO14443A_Card.SAK & 0x20 ) != 0x00 ) && ( tagsToFind & TRACK_NFCTYPE4A ) )/* TT4A */
return TRACK_NFCTYPE4A;
}
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Looking at line The first argument `
ISO14443A_Card.SAK & 0x20 ) != 0x00`
Passes but the next argument ( tagsToFind & TRACK_NFCTYPE4Afails
..... strange.tagsToFind is 0xFF
TRACK_NFCTYPE4A is 0x08
Hmmmm. 0xFF & 0x08 does not evaluate to 0.... OK, I'll separate them and make sure which one is failing.
if ((tagsToFind&TRACK_NFCTYPE2) || (tagsToFind&TRACK_NFCTYPE4A))
{
PCD_FieldOff();
HAL_Delay(5);
ISO14443A_Init( );
if(ISO14443A_IsPresent() == RESULTOK)
{
if(ISO14443A_Anticollision() == RESULTOK)
{
if ( ( ( ISO14443A_Card.SAK & 0x60 ) == 0x00 ) && ( tagsToFind & TRACK_NFCTYPE2 ) ) /* TT2 */
return TRACK_NFCTYPE2;
if( ( ( ISO14443A_Card.SAK & 0x20 ) != 0x00 ) ) // && ( tagsToFind & TRACK_NFCTYPE4A )
{
if( ( tagsToFind & TRACK_NFCTYPE4A ) )
{
return TRACK_NFCTYPE4A;
}
}
}
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
What do you know, against all odds and CS universal laws, line 15 evaluates to 0. This must be a sick joke right.
So just for giggles, I add an else:
if ((tagsToFind&TRACK_NFCTYPE2) || (tagsToFind&TRACK_NFCTYPE4A))
{
PCD_FieldOff();
HAL_Delay(5);
ISO14443A_Init( );
if(ISO14443A_IsPresent() == RESULTOK)
{
if(ISO14443A_Anticollision() == RESULTOK)
{
if ( ( ( ISO14443A_Card.SAK & 0x60 ) == 0x00 ) && ( tagsToFind & TRACK_NFCTYPE2 ) ) /* TT2 */
return TRACK_NFCTYPE2;
if( ( ( ISO14443A_Card.SAK & 0x20 ) != 0x00 ) ) // && ( tagsToFind & TRACK_NFCTYPE4A )
{
if( ( tagsToFind & TRACK_NFCTYPE4A ) )
{
return TRACK_NFCTYPE4A;
}
else
{
return 1;
]
}
}
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
AND THE HEAVENS HAVE OPENED, Now line 15 evaluates to
TRUE / 1
...... But wait... what just happened.... So I remove the else and what do you know.... line 15 is back to evaluating false again.....I think my sweet little STM32L476 is possessed by demons and I need to exercise some digital god rituals or something.