Skip to main content
Associate II
July 2, 2024
Question

Heap size for STM32F101RG

Hello,

I have a question on how to optimally configure the RAM of the STM32F101RG.

The controller has 1MByte Flash, 80KByte RAM. I need to use most RAM for Heapsize and I configured within Keil IDE under target options/ASM

0xCD00 for Heap size and

0x1000 for Stack size. Totally, the size is much smaller as 80 KByte. But when I try to increase the size for the Heap only a little bit, I get errors like

: No space in execution regions with .ANY selector matching

 

Within scatter file, I configured in this way:

</

LR_IROM1 0x08000000 0x000FA000 { ; load region size_region
ER_IROM1 0x08000000 0x000EA600 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM1 0x20000010 0x00014000 { ; RW data
.ANY (+RW +ZI)
}
}

 

/>

How can I optimally use the 80KBytes of RAM for a large heap?

Thanks in advance!

Best regards,

Regina Kaune

This topic has been closed for replies.

2 replies

Douglas MILLER
ST Employee
July 2, 2024

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

Associate III
December 16, 2024

Hello @Douglas MILLER 

I'm using a different processor(STM32H757) and adding software packs(COMSIS RTOSv2, OpenAMP), but this post seems to be the answer to my problem because it's the best way to use RAM for a large heap.

Could you help me please?

 

# Post Name : STM32H757 / RTOS / OpenAMP / Memory "._user_heap_stack " Size Saturation

# Post Link : https://community.st.com/t5/stm32-mcus-embedded-software/stm32h757-rtos-openamp-memory-quot-user-heap-stack-quot-size/m-p/753062