Skip to main content
ANDRE THEVENIN
Associate
June 28, 2018
Question

HCD_HandleTypeDef has 15 channels

  • June 28, 2018
  • 1 reply
  • 642 views
Posted on June 28, 2018 at 19:09

On STM32F7, the HS interface has 16 host channels.

But in the HAL, the HCD_HCTypeDef structure has only 15 HCD_HCTypeDef items.

Is this normal ?

Is this a bug ?

Is there an hidden reason ?

(I have an application which can have the need on the 16 channels because several devices will be connected via a hub)

#hcd_handletypedef #hcd_hctypedef
    This topic has been closed for replies.

    1 reply

    Khouloud GARSI
    ST Employee
    July 5, 2018
    Posted on July 05, 2018 at 15:23

    Hi

    ANDRE.THEVENIN

    ?,

    The issue is confirmed. We will fix it and update the &39&39stm32f7xx_hal_hcd.h&39&39 ASAP.

    Many thanks for bringing this point to our attention

    I also advise you to refer to the application note

    https://www.st.com/resource/en/datasheet/stm32f479ii.pdf

     which will help you to build your own USB application based on an STM32 MCU. If you have any feedback about the application note, please do not hesitate to share it here:

    https://community.st.com/0D50X00009XkVtDSAV

    On the FAQs section, the following question was answered:

    0690X0000060LC6QAM.png

    Khouloud.