Skip to main content
Ricardo Hassan
Associate III
Aug 30, 2018 10:59 PM UTC
Solved

Have I found a driver issue?

Greetings,

I'm using an STM32L496. I have a peripheral connected to PE11, which I have configured as an interrupt on the rising edge. I have another circuit connected to PA11, which is normally an input. So far no problem. In order to do a self test, I briefly configure PA11 to a rising interrupt as well, then when the test is over I switch it back to an input. This has the side effect of also disabling the interrupt on PE11. I have to explicitly reconfigure the GPIO settings for PE11 to get the interrupt working again. It seems like there is an issue in the HAL driver that is failing to handle the GPIO port correctly. Has anyone seen this behavior?

Ricardo

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 30, 2018 11:32 PM UTC

Not really the EXTI can only deal with one GPIO Bank per pin position. ie 11 can be ONE OF A, B, C, D, E , F ,G, etc. You get to manage which, the driver doesn't get to remember, the GPIO Init structure is transient.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 30, 2018 11:32 PM UTC

Not really the EXTI can only deal with one GPIO Bank per pin position. ie 11 can be ONE OF A, B, C, D, E , F ,G, etc. You get to manage which, the driver doesn't get to remember, the GPIO Init structure is transient.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..