Skip to main content
Gudgel.boB
Senior
December 25, 2019
Question

Has anyone successfully ran an STM32F4xx CANBUS at 500K baud ?

  • December 25, 2019
  • 10 replies
  • 3284 views

We are using the STM32F446 at 180 MHz and one of my engineers says he can't quite get the CAN peripheral to run at 500K (reliably?) with the available clocking system.

Anybody know any tricks to make this work ?

This is partly what he said.....

"I don't think running the AHB bus @180 MHz will work for 500K baud CAN communications. It kinda sorta works but the prescalers and time quanta settings I have to work with won't let me get quite close enough to 500K baud for it to be reliable. Too many errors. It's still preliminary right now, but it doesn't look good. If I set the N parameter in the PLL to 200 (rather than 180) I can get AHB / AHP1 / AHP2 buss frequencies of 200 / 100 / 50, which violates the requirements in section 6.3.3 but I can get the CAN frequency right on 500K baud. This appears to work but technically I'm overclocking the part."

This topic has been closed for replies.

10 replies

T J
Senior III
December 25, 2019

I guess you are trying to attach to an existing canBus of 500KHz.

please make sure you have ABOM turned ON and the canBus line impedence is below 200R ( 60R is the correct line impedence)

You will have to use a crystal for reliable stable frequencies.

You may have to drop your frequency down to match the 500khz exactly.

you can over clock the unit slightly, but it is not recommended if you are working anywhere near the maximum temperatures.

You can read the onboard die temperature, if it is below 60C you should be ok to overclock slightly.

Better to under-clock to match the 500k exactly and stay within the ST recommended operating conditions.

turboscrew
Senior III
December 27, 2019

I've used 1MBPS CAN on F427.

Gudgel.boB
Senior
December 29, 2019

Thanks guys. I guess I will find out after the 1st of the year what the engineer's issue REALLY is.

I see calculations for Qt or is it Tq (quantum time) which comes out pretty close or perfect to 500K from an AHB of 45 MHz.

But then there are 2 more calculations for 2 register values that also involve Tq to come up with more possible issues regarding how things sync up.

I guess that CAN is just not as simple as a USART for calculating BAUD rate or bit rate.

turboscrew
Senior III
December 29, 2019

With high speed, the number of well-working combinations of prescaler and time quanta becomes quite limited.

In my case (1 mbps), I recall, there was just one.

turboscrew
Senior III
December 29, 2019

Found my old notes...

PCLK = 45MHz, 1/45 us = 22,22 ns

1Mbps = 1 bit/us

1000ns/22,222 ns = 45,000045

=> 45 PCLKs per bit; 45 = 5*3*3

1 Mbps:

Prescaler = 5, 1 + 2 + 3 + 3 = 9

(22,222ns * 5 * 9 = 999,999ns)

Numbers in registers need to be one less than the value used

prescaler = 4 (5-1)

(SYNC_SEG is always 1)

TimeSeg1 = 4 (2+3-1) (PROP_SEG + PHASE_SEG1)

TimeSeg2 = 2 (3-1) (PHASE_SEG2)

turboscrew
Senior III
December 29, 2019

Made that to 500 kbps by doubling the prescaler.

Gudgel.boB
Senior
December 30, 2019

Thanks for digging out your notes, turbo ! I sent this off to the guys. Hopefully it can help !

Happy new year !

Gudgel.boB
Senior
January 4, 2020

We have successfully ran this part at 500K now.

He found 3 different number combinations that work so far.

Thank you VERY much folks for your help !

This is great !

Happy new year !

SGeni.1
Associate
January 8, 2020

Can you please help me on this topic also? We are using an STM32F7XX board and we have problems with transmission

Gudgel.boB
Senior
January 8, 2020

Looks like there are 3 (three) combinations of numbers that will work at 500K baud reliably with the processor running at 180 MHz.

Remember that the CAN bus peripheral runs at 45 MHz and not 90 MHz

Check Turboscrew's initialization above as well.

I will get the other numbers here that should work as soon as I talk to Jim, the guy working on this.